Connect to your HMI straight to your smartphone or tablet
Vijeo Design’Air Plus is Schneider Electric’s new remote access feature in Vijeo Designer offered as an application for tablets and smartphones. Vijeo Design’Air Plus enables you to create a tablet/smartphone project specifically for the tablet/smartphone display size. At runtime, using this project, an operator can access the HMI to display data and control automation processes from the tablet/smartphone.
Vijeo Design’Air Plus provides operators with the capability to select a user application, and on successful login, download and launch the tablet/smartphone application. The operator can view and monitor an automation process, and for example, change values in numeric displays and string displays. In the Alarm Panel, the operator can monitor and acknowledge alarms.
You can use Vijeo Designer’s drawing tools to create and edit a visual representation of the automation process. You can draw shapes and parts (such as rectangles, arcs, pies, numeric displays, switches, and bar graphs), use the gradient feature to enhance the color of the drawn objects, and set up an Alarm Panel for remote alarm monitoring and interaction.
Requirement:
Vijeo Design'Air Plus requires Vijeo Designer V6.2 or later on your HMI targets
Limitations
Target families not supported: XBTGT1000 Series, XBTGC Series, HMISCU Series
Discover the HMI product range