How can we help you today?

Can we perform Automatic Transfer switch (1out of 2) using withdrawable version from MCCB of type NSX ?

- The ATS (Automatic transfer switch 1 out of 2) using the NSX MCCB can only be performed using:

1- Fixed MCCB NSX
2- plug in MCCB NSX

Attached here Catalog pages illustrate this info as well as connections for NSX ATS

Schneider Electric United Arab Emirates

Attachment(s)
100 TO 630 NSX Source Changeover Assembly 00999531A 01.pdf [2.65 MB]
Source Changeover.pdf [361.89 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre