How can we help you today?

In Sepam catalog one of the phase current inputs characteristics is "1 second overload". What does it mean? Should it be considered while sizing the current transformers used with Sepam?

Issue:
Customer wants to know what does the below technical characteristic for the current input of Sepam 80 mean

one second overload C/Cs

Environment:
Sepam general characteristics

Resolution:

One second overload means the Sepam phase current input can't withstand more than 500A during 1second. If Sepam current input is subjected to a greater value of current, this could destroy the relay. Accordingly, this condition must be considered while choosing the current transformer.