How can we help you today?

Why are 9001KM38 listed twice, as resistor and full voltage light modules?

Issue:
Is the 9001KM38 a resistor type or full voltage type of light module?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony Pushbuttons

Cause:
Product Features

Resolution:
Both descriptions are accurate. They are both the same device but can be selected by either description depending on the application/preference.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre