Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the coil consumption or burden for the Tesys LC*D** contactors? 09 through 38
Issue:
Coil consumption or burden for the Tesys LC1D/2D contactors from 9A - 38A

Product Line:
Contactors and Starters - IEC

Environment:
Tesys D Contactors

Resolution:
All AC coils for the LC1D09 through LC1D38 3-pole contactors ( including ring tongue, quick connect and spring terminal versions ) have an inrush of 70 volt-amps for either 50 or 60 Hertz applications, and a sealed value of 7 volt-amps for 50Hertz applications or 7.5 volt-amps for 60 Hertz applications.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings