Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which contact blocks are used with XAL control stations?
Issue:
XAL Control Station contact blocks

Product Line:
Push Buttons and Operator Interface

Environment:
XAL Control Stations

Cause:
It is unclear which contact blocks are used in 22mm control stations

Resolution:
The ZENL contact blocks are used in these control stations.  These blocks mount directly to the control station itself and do not use a mounting collar.  A normally open contact block is ZENL1111, and a normally closed contact block is ZENL1121.

These contact blocks are rated 10 amps max, AC-15 A600 and DC-15 R300

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings