How can we help you today?

Which contact blocks should be used with the ZB4BA7*** two, and three head operators?

Issue:
Which contact blocks should be used with the ZB4BA7*** two, and three head operators?

Product Line:
XB4/ZB4 22mm Operators

Environment:
All Product Lines

Cause:
Can not find it in the Digest

Resolution:
Use the standard ZBE101 for NO, and ZBE102 for NC.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre