Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to setup an OPC connection for M241 PLC using OFS configuration tool?
Currently, it is not possible to setup an OPC connection for M241 PLC using OFS configuration tool. Therefore, an alternative OPC-DA tool will be required.

Please note, M241 PLC can only be used as an OPC server, therefore, perhaps you can try available OPC clients for communications.

You can have as many OPC servers as you want in one machine, it comes down to the OPC client and which one it will connect to for data. Some clients allow to configure multiple servers so you can communicate to multiple OPC servers at the same time. It all depends on your OPC client tool.

Schneider Electric Australia

Attachment(s)
Catalog Communication via modem and router with Modicon M221 M241 M251 logic controllers English 2017.pdf [1.29 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings