Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I test PLC client and PLC server communication with explicit messaging using Control Expert’s simulator instead of actual hardware?
The solution is to use the steps below which show the setup of Control Expert V15.0 and above’s IP address port simulator.
Step 1: Create an XML file with the format below. Any IP address can be used and assigned to a port.

eg).
<EquiList>
<PLCAdressSim Address="192.168.250.1" Port="502"></PLCAdressSim>
<PLCAdressSim Address="192.168.100.1"  Port="503"></PLCAdressSim>
</EquiList>

Step2: Open Control Expert and create a new M580 project. Create a program with the Read_Var block and assign an IP address that corresponds to one of the ports (created in the XML). Eg)


Build and connect to the simulator using the port number not assigned to the IP address used in the ADDM block. Transfer the program and run. Eg)



Step 3: Open another instance of Control Expert and create another blank M580 project. Connect to the simulator as below. The IP address must be 127.0.0.1 but the port number must be the one assigned to the IP address used in the ADDM block previously.



Step 4: From the task bar, select Options from the Simulator menu


Step 5: Enter the location of the .xml file


It will now be possible to monitor the memory read in by the Read_Var block.

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings