Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to deactivate ATVLogic running in ATV320 drive?

The ATVLogic could be deactivated by "Disabling the function" (FBCD) or the logical input that start the ATVLogic Mode (FBRM).

- Set FBCD to STOP, this will deactivate the ATVLogic function:

By keypad:

Go to Drive menu/ Configuration/ Full/ Function blocks, then set FBCD to STOP.
image.png

By SoMove:

Connect the SoMove to the drive, then set FBCD to STOP.
image.png

- Check by keypad or SoMove which logical input (LIx) is set to FB start mode, then disable it.

In the above example, when LI3= OFF, the ATV logic is disabled.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings