How can we help you today?

How is the C-Bus Controller Powered?

The C-Bus Controllers can be temporarily powered using a USB-A to USB-B cable via the USB-B port on the front of the controller; however, this only provides limited functionality.

For full functionality the C-Bus Controllers require 24VDC

Power Supply

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre