Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to download the C-Bus Toolkit 1.17.2?
Where to download the C-Bus Toolkit 1.17.2?

Release Date: 11/01/2024
Version: V1.17.2
Reference: C-Bus_Toolkit_V1.17.2
C-Gate: 3.2.3 (build 1760)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10, Windows 8, Windows 7

Bug fix:
  • Fixed an issue in the Edit Network dialog that prevented the network from being opened or scanned when the interface type was changed from Serial to C-Bus Home Controller.
Updates to C-Gate include:
  • Support firmware version 1.3.0 of DIMDD4 (5504D2D) and DIMDD8 (5508D1D) C-Bus Digital Dimmer devices.

Link to download C-Bus Toolkit 1.17.2
https://www.se.com/au/en/download/document/C-Bus-Toolkit_V1.17.2/

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings