Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to download the C-Bus PICED 4.15.1?
Where to download the C-Bus PICED 4.15.1?

Release Date: 18/01/2024
Version: V4.15.1
Reference: PICED-V4.15.1
C-Gate: 3.2.3 (build 1760)
Operating systems: Windows 11 Professional (64-bit), Windows 10 Professional (64-bit), Windows 10 Enterprise (64-bit), Windows 10, Windows 8, Windows 7

Fixes
  • Fixed an issue where the leading \\ in UNC paths were being replaced with a single \ after restoring a project
  • Adjusted the file filters for the Transfer Other Configuration Data File option in the Export Project dialog to clear up any misunderstanding about the files that can be selected

Link to download C-Bus PICED 4.15.1
https://www.se.com/au/en/download/document/PICED-V4.15.1/

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings