Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Alarm Priority in Power Monitoring Expert

Issue

When creating a filter for Alarm priority, how do I determine what is a priority alarm or not?

Product Line

EcoStruxure Power Monitoring Expert

Resolution

The priority of an alarm or event can be configured in the PME system. The typical PME alarm priority categorization is:

  • High priority alarm: 193 - 255
  • Med priority alarm: 128 - 192
  • Low priority alarm: 64 -127
  • Information: 0 - 63

The alarms are located in the below location in the predefined events file

C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\translators\events

Schneider Electric Australia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings