Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to do Modbus Termination for Interface module, ComPacT NSX, Modbus SL HUB LV434224

Product:

Interface module, ComPacT NSX, Modbus SL HUB LV434224

Resolution:

Terminal VW3A8306RC, you can insert it to any port of the three ports on the final Modbus SL hub. If all ports are occupied, You can use the terminal block VW3A8306DRC connector to add the termination as shown in the second picture below.

Image 1

The terminal VW3A8306DRC, you need to connect it only to the final Modbus SL hub.

Image 2

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings