Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
DCBMWizard, why can I only scan line A on each DALI power supply DCDALCIP250-2 using the DCCABKIT6 programming cable?

Confirmed that DCBMwizard can only connect to LineA

To connect to LineB

1) You can remove LineA and move LineB to LineA. Once commission is completed you can rewire it back.

2) or having a secondary DCCABKIT6 programming cable as  line B is powered by line A

Schneider Electric Australia
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
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings