Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the inductive rating for the contactor A9C22715??

According to the datasheet:

Utilization categories:

AC-7a (resistive loads): 16 A

AC-7b (inductive loads, small motors): 6 A at 250 V AC

See below link for further information.

Image

A9C22715 - iCT 16A 1NO 1NC 230...240V 50Hz contactor | Schneider Electric New Zealand

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings