How can we help you today?

How does the ION 9000 meter measure / calculate the primary frequency of the power system it is connected to and measuring?

Issue:

How does the ION 9000 meter measure / calculate the primary frequency of the power system it is connected to and measuring?

Resolution:

The ION9000 measures primary frequency based on the fundamental component of the voltage waveform. The zero-crossing method is a simpler approach often used in basic meters, where frequency is calculated by measuring the time between successive zero crossings. However, the ION9000 uses DSP techniques, including FFT, to extract the fundamental frequency accurately even under distorted conditions. This is because FFT allows precise separation of the fundamental from harmonics and interharmonics.

Since the ION9000 complies with both standards (IEC 61000-4-30 & IEC 61000-4-7), it is safe to assume that it uses FFT for harmonic analysis and likely the same process for frequency measurement.

Please refer to the attached technical documentation for more detailed explanation

Schneider Electric Australia

Attachment(s)
IEC 61000-4-30 compliance and ION meters technical note (3).pdf [112.39 KB]
ION9000- Technical Data Sheet (2).pdf [2.86 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre