Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Domain Accounts are unable to access the PME 'Reports' application

Issue
Domain accounts logged in to the PME server are unable to access the 'Reports' application.

Resolution

The domain controller was not accepting 64-bit requests, so to resolve this you need to enable 32-bit Applications in the Webreporter App pool in IIS.

On the PME server: Open Internet Information Services (IIS) Manager. In the left pane, expand server name > Application Pools. Right-click the WebReporter AppPool > Advanced Settings > set "Enable 32-Bit Applications" = True. Click OK, and right-click the Application Modules AppPool > Start (or if already running, do Stop, then do Start)

Run the command prompt as administrator and reset the iis with the command: iisreset

    Restart the ION Appmod services.

    Schneider Electric Australia

    Explore more
    Product:
    Users group

    Discuss this topic with experts

    Visit our Community for first-hand insights from experts and peers on this topic and more.
    Explore more
    Product:
    • Products Documentation
    • Software Downloads
    • Product Selector
    • Product Substitution and Replacement
    • Help and Contact Centre
    • Office Locations
    • Where to buy
    • Phone: 13 73 28 (13 SEAU)
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
    • Terms and Conditions of Sale
    • Change your cookie settings