How can we help you today?

Is there a profile for the Easergy T300 in EcoStruxure Power Operation?

Issue
Is there a profile for the Easergy T300 in EcoStruxure Power Operation (EPO)?

Resolution

EPO includes a profile for the Easergy T300. Please refer to the image below from EPO Profile editor.

Screenshot of Easergy T300 profile in EPO

Both the DNP3 and IEC 104 protocol are supported and you can choose either of the protocols. From the T300 side you have to make the default config from T300 Generator with selection of protocol.

Please make sure the variable addressed are the same in T300 coreDB and in the PO profile editor.

​​​​​​​

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre