How can we help you today?

In PM5320 is it possible to change the Modbus ID from 255 when connecting via ethernet so that it can be integrated to SCADA

Product Line:

METSEPM5320

Resolution:

PM5320 have ethernet with Modbus TCP/IP. 255(0xFF in Hex) is not the device address. It's the unit identifier.

As per Modbus TCP/IP standards, unit id for standalone meter should be 255. The unit id of PM5320 and PM5340 meter is 255 and it cannot be changed.

You can see the excerpt below taken from Modbus standard

Image

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre