How can we help you today?

How to update M580 PLC project firmware from Version 1.1 to SV 2.0?

Issue:

When trying to update the M580 PLC firmware in Control Expert from version 1.1 to SV2.x or later , we are getting the following errors ,

Error_Message

Product Line:

M580 PLC Range .

Resolution:

Please Export the project file (that has got M580 Project firmware as SV 1.1) to .ZEF and then please search for M580 CPU Change V1V2 Software from Windows Search bar (this software is an Add-ons that comes along with Control Expert) and open the software.

M580_CPU_from V1.1 to V2.0

Please import the .ZEF file and click Next and the Converted application will be automatically saved to location in which the previous firmware version file located . The converted application will have a following words added to application name "L2"(for example : Test_L2.ZEF)

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre