How can we help you today?

Why is there 750mm space required from the wall when installing a VarSet capacitor bank?

The cooling occurs from the front and top of the unit. The 750 mm space is optional and is intended to provide access for removing the rear cover in case any maintenance is required on the components assembled at the rear side (e.g., tightening of the detuned reactor cable). However, most maintenance activities can be performed from the front side with the proper tools.

Image1

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre