How can we help you today?

Selecting Between BMXNOC0401 and BMXNOC0401.2 Modules in Control Expert

FAQ question:

How do I know whether to select the BMXNOC0401 or the BMXNOC0401.2 module in Control Expert, and what happens if I choose the wrong one?

FAQ answer:

The BMXNOC0401.2 is the same physical hardware as the BMXNOC0401 but includes firmware version 2.01 or higher, which unlocks additional features. You should select the module variant based on the capabilities supported by your CPU and the firmware on your physical NOC module.

Key differences:

  • Email Service (SMTP): Available only on BMXNOC0401.2, allowing the PLC to send email notifications using the SEND_EMAIL block.
  • Network Time Protocol (NTP): Only BMXNOC0401.2 supports NTP time synchronization.

Requirements to use BMXNOC0401.2:

  • Your CPU must be a BMXP342..... model (e.g., BMXP3420302).
  • The physical NOC module must have firmware v2.01 or newer.

Behavior if the wrong variant is selected:

  • Selecting BMXNOC0401.2 without meeting the above requirements results in a compatibility error or download failure.
  • Selecting BMXNOC0401 when BMXNOC0401.2 is supported is safe, you simply won’t have access to email or NTP features.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre