How can we help you today?

Control Expert V15.3 Silent (Automatic) Installation

Issue:

How to install Control Expert V 15.3 in Silent (Automatic ) Mode ?

Product Line:

Control Expert V15.3

Resolution:

Automatic installation of Control Expert requires no action during the installation. The installation performed is the same as a default installation in manual mode.

It is carried out with the provided install.bat batch command file. This file is at the root of the Control Expert DVD-ROM or in the installation package (.iso file).

Control Expert V15.3 Install_Bat for Silent Install

Please see the below Steps :

1.Please mount the installer file (the original installer file from our Website) , then press Control +A (to copy the whole contents) on to your PC.

2.Edit the Install.bat file that you have copied to adapt the modifiable parameters to your needs/configuration.

3. Firstly please copy the installer contents path of the folder that is in your PC and paste it to Install.bat file .

Set_Directory

4.Secondly Please leave the installation destination folder path by default .

Set_Installation_Path

5.By default the Installation Language is English , but you can to below languages according to your needs

Set_Language

6. Next , please Set Driver Install to yes and SESU (Schneider Electric Software Update) to yes

Set_Driver_SESU

7. Next please Agree with EULA (End User License Agreement) and Save the Changes.

Set_EULA

8. Finally , please Right Click and Run the Install Bat file as Run as Admin.

Schneider Electric Australia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre