How can we help you today?

What is the correct register to read Digital Input status for PM5560?

Product Line: Power MetersPM5000 series

Environment: METSEPM5560, METSEPM5561, METSEPM5563, METSEPM5580, METSEPM5650

Resolution:

For PM5560, the digital input status can be read in two ways:

Image

1. Register read

- Register 2401

- Bit 0 = DI1

- Bit 1 = DI2

- Bit 2 = DI3

- Bit 3 = DI4

2. Coil read:

- Coil 38416 = DI1

- Coil 38417 = DI2

- Coil 38418 = DI3

- Coil 38419 = DI4

So, to read the current status of the digital inputs:

- use register 2401 to read all four DI statuses in one value

- use coils 38416 to 38419 to read each DI individually

- The data type for register 2401 is BITMAP & it’s a 16bit register

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre