How can we help you today?

NS1250N ML5.0E not reading frequency and showing zero Power readings.

Issue: Micrologic 5.0E displays NaN when reading frequency and shows zero power readings when the current is below a certain threshold.

Product Line: Micrologic E trip units installed with Compact NS breaker

Environment: Micrologic E Trip Units

Resolution:

According to the user guide,Micrologic E trip units do not support frequency display. Therefore, frequency values are not available when using this trip unit.

For confirmation, please refer to the provided link, page 66.

https://download.schneider-electric.com/files?p_Doc_Ref=DOCA0218EN&p_enDocType=User+guide

Image1

A check of the register list for Compact NS breakers (refer to the attached screenshot) confirms that Compact NS units equipped with Micrologic E trip units do not support frequency display. As a result, the frequency register returns NaN.

In the register table, the A/E/P/H column applies to NT/NW and NS breakers. This table indicates that only P and H trip units support frequency measurement and display on the registers. Micrologic E trip units do not include this capability.

For further details, please refer to the linked document, page 91.

https://www.productinfo.schneider-electric.com/compactnsxmodbuscommguide/compact-nsx-modbus-comm-guide/EN/DOCA0091EN-09.pdf

Image 2

For the Issue regarding incorrect power readings:

On Micrologic 2.0E, 5.0E, and 6.0E trip units:

The power value displayed on the Micrologic E front display and transmitted via Modbus is reported as zero when the load current is below 0.07 × In, where In represents the rated input current.

The current value displayed on the Micrologic E front face and transmitted via Modbus is reported as zero when the load current is below 0.005 × In.

When the load current falls between 0.005 × In and 0.07 × In, and the voltage is non‑zero, the current and voltage values are displayed normally; however, the calculated power value remains zero.

As a result, in customer applications, power calculation effectively begins when the load current exceeds 0.07 × In (Ia).

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre