How can we help you today?

What do the terms PWH1 I1 and PWH1 V1 mean in the Power Harmonics module?

Product Line: ION 9000 Power meters

Environment: METSEION92030

Resolution:

Explanation of Power Harmonics Angle Parameters

The parameters PWH1 V1/V2/V3 Angle and PWH1 I1/I2/I3 Angle are sourced from the Power Harmonics module under the Fundamental Power group. These parameters represent the phase angles, measured in degrees, of voltage and current for each phase at the fundamental frequency.

Image

  • PWH1 V1 Angle → Phase angle of Voltage Phase A
  • PWH1 V2 Angle → Phase angle of Voltage Phase B
  • PWH1 V3 Angle → Phase angle of Voltage Phase C
  • PWH1 I1 Angle → Phase angle of Current Phase A
  • PWH1 I2 Angle → Phase angle of Current Phase B
  • PWH1 I3 Angle → Phase angle of Current Phase C

These values are commonly used for power quality analysis and phase relationship verification at the fundamental frequency.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre