How can we help you today?

Can you reset an Ap LED light on the ComPacT NS micrologic trip unit?

Product Line: Micrologic Trip units for ComPacT NS  & MasterPact NW fixed and drawout types

Environment:Micrologic 2.0 A & E, Micrologic 5.0, 6.0, 7.0 A E & P types

33532, 33526, 33533, 33534

Resolution:

img

The AP LED is a self-protection/self-diagnostic indicator.The following are possible causes for Ap LED to lit up:

  • The 24 VDC power supply voltage may not be stable. Sudden voltage drops and recovery can cause communication loss between the internal ASIC protection chip and the MCU.
  • Presence of an EMC-generating source nearby, such as large capacitor switching (reactive power compensation systems) or frequency converters.
  • Loose connections between the Micrologic unit and the current rating sensor lug, or at the rear-side trip unit base terminals.

Important point about clearing Ap LED

  • If there is no tripping and the AP LED remains lit, the protection function is still operational. Pressing the reset button can clear the AP LED indication without compromising any protection features on the breaker.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre