How can we help you today?

How to connecting M580 via https through NOC0301

Rack

Step 1:

Enable backplane port from NOC Advanced Configuration.

Backplane

Step 2:

Enable Https on both PLC and NOC, make sure firmware version of your PLC is >=4.30

Https

Https

Step 3:

Once step 2 is done, you shall be able to ping your PLC port 443.

Ping 443

Step 4:

Open Security Editor, first click Generate Self Signed Certificate

Security Editor

Step 5:

Then in Certificate whitelist, select PLC IP address then click Trust Certificate then apply.

Certificate

Step 6:

Then Connect PLC via Https

Connection

Success

Summary:

When trying to connect PLC via Https, the Https server is in the M580 not in the NOC0301. (NOC doesn't have https server embedded), so always need to use the IP address of PLC (Not NOC) to establish https Communication. It is possible to plug ethernet cable into the port from NOC module but still when connect from PC, still need to use PLC IP address. Ping 443 port with NOC IP address will always fail, because NOC doesn't have https server embedded. Ping 443 port with PLC IP address will work if backplane port is enabled. This way, the https communication is going from NOC module through the backplane and eventually reached PLC https server.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre