How can we help you today?

Aside from the new generation C-Bus Digital Dimmers, Voltage-Free Relays & eDLT firmware v 2.x, what other devices can be configured using C-Bus Commission?

As of C-Bus Commission v2.15.0 the following wizards are supported in Global Programming C-Bus devices can be loaded into the Properties window and configured:

  • 30/40 Series Modules: 5031NMML, 5041NMML
  • PIR Sensors: 5753L, 5754ODPE, 5751L & 5750WPL
  • Bus Couplers: 5104BCL & 5102BCLEDL
  • Fan Controller: L5501RFCP
  • Auxiliary Input Unit: L5504AUX
  • Extra Low Voltage Relay: L5108ELVP
  • Shutter Relay: L5501RBCP

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre