How can we help you today?

Values within a EPO 2022 project are misbehaving during project runtime

Issue
Values within a EPO 2022 project have been misbehaving when attempting to start a project runtime within a production environment. The values seem to be getting corrupted/changed when services stand up during a recompile. The values being changed effect DBFs:
System Model > Alarms > Analog Alarms
System Model > Alarms > Advanced Alarms

It was also noted that the 'High' alarm threshold values were automatically changing from 1 to 3.40e+38, and alarm delays were reverting to 0 (00:00:00), causing nuisance alarm flooding and preventing breaker state change events from being captured.

Resolution

  • We identified the issue was caused by the [Alarm]UseConfigLimits parameter set to 1 in the Citect.ini file, which prevented proper synchronization of alarm property changes between redundant servers.
  • We recommended setting [Alarm]UseConfigLimits = 0 to allow changes made offline in the project to deploy correctly with restarts on Standby and Primary servers.
  • We also provided details of two related bugs: 3045403 (fixed in EPO2022 CU7 and EPO2024 CU2) and 4003810 (fixed in EPO2024 CU3, not fixed in EPO2022) affecting writable alarm properties with UseConfigLimits=1.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre