How can we help you today?

How can the correct communication port be identified for EVlink chargers, and where can the configured port be verified?

Product Line: EVlink EV Charging Equipment (EVCE)

Environment: EVlink chargers commissioned with OCPP communication profiles

Resolution: The recommended communication profile is Security Profile 2 (port 9982). However, the communication profile is automatically configured by the EVCE during charger commissioning, so no manual action is required from the customer.

Available communication ports:

  • WS (not recommended): 9979
  • WSS Security Profile 0: 9980
  • WSS Security Profile 1: 9981
  • WSS Security Profile 2 (recommended): 9982

Verification: If verification is required, the customer can use eSetup or ECCT and review the Supervision Configuration. The configured port indicates which Security Profile is currently in use.

**Important Note: Do not manually modify the configured port. The EVCE stores the selected communication profile and validates it during operation.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre