How can we help you today?

How to Set an IP-Address on TeSys-T using an M580 PLC DHCP Server

Product Line:

Tesys-T Motor Controller .

M580 PLC Product Range.

Resolution:

There are quite a few ways to set the IP address in an LTMR__E_ device and one off them is using an M580 PLC DHCP Server

Using DHCP Server

  1. Set the Rotary Switches on the TeSys T.
  2. Creating M580 PLC and add the TeSys T DTM .
  3. Add TeSys T ,Device Name to DHCP Server .
  4. Build and download the M580 Application.
  5. Verify the assigned TeSys T address

NOTE:

Please refer the TeSys T Guide Page no 30-31 for more details on Rotary Switches & Device name.

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre