How can we help you today?

How to resolve "S_SYST_CLOCK_MX is not supported on this PLC" Error Message

When import S_RD_ETH_MX and S_RD_ETH_MX blocks into a Safety PLC program with wrong firmware version, you will get below Error Message.

Error Message

If you then remove S_RD_ETH_MX and S_RD_ETH_MX blocks from the project, you will see S_SYST_CLOCK_MX error still remains.

Error Message

If you then trying to find and delete this block, you will find that S_SYST_CLOCK_MX is not used anywhere. Cross-reference doesn't return any result.

Search returns null

Below is the solution:

S_SYST_CLOCK_MX is actually automatically created when you insert S_RD_ETH_MX or S_WR_ETH_MX block into project. To remove it, first you need to fully delete S_RD_ETH_MX and S_WR_ETH_MX from your project. Please see below steps:
Solution
Once these two blocks are fully deleted. Please export your project as ZEF

Export
Last, you can open this .ZEF file and then you can build it without error message.

Result

Schneider Electric Australia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Office Locations
  • Where to buy
  • Phone: 13 73 28 (13 SEAU)
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
  • Terms and Conditions of Sale
  • Change your cookie settings
  • Preference Centre