From the drawings received I see that the circuit breaker is supplied from the bottom side. As I understand, your request concerns this device.
The power sign is needed to be changed in this situation.
It can be done directly on the Micrologic X trip unit. Please refer to the FAQ linked below:
See link:
https://www.se.com/us/en/faqs/FAQ000267169/
To set the power sign on an MTZ control unit, on the MicroLogic X display screen navigate as follows:
Home > Configuration > Network > Power sign. The setting may be toggled from + to - or vice versa.
The power sign may also be changed with EcoStruxure Power Commission software.
It can also be done using Ecostruxure Power Commission software. Please refer to the video below:
See link:
https://www.youtube.com/watch?v=Zs_XPfwOqeM
+++ +++ +++
Where to download Ecostruxure Power Commission prequisite or installation guide:
See link:
https://www.se.com/us/en/product-range/62980-ecostruxure-power-commission/#documents