Issue
What will happen to the analog outputs on the AS-B872-100 go to on a loss of communications to the drop?
Product line
Modicon 1/2/3/4/5/8/984
Environment
AS-B872-100
Resolution
The stop state behavior of the module is set via a 4 position dip switch bank located at the rear of the module. The bank contains 4 switches (1 four each respective channel on the card). If set to the 0 position (left) the channel will return to a 0 state on communications failure. If set to the 1 position (right) the channel will hold last value on a communications failure.
Publié pour: Schneider Electric Belgium