The input to a counter module can be attached to a High Speed output module, and it will count the High Speed results. The output of the counter module, however, will only update once per second.
For example if the input is pulsing 12 time per second the output will be:
| Time (s) | Input pulses | Output Register of the Counter module |
| 0 | 0 | 0 |
| 1 | 0 | |
| 2 | 0 | |
| …. | 0 | |
| 1 | 12 | 12 |
| 13 | 12 | |
| 14 | 12 | |
| …. | 12 | |
| 2 | 24 | 24 |
| 25 | 24 | |
| 26 | 24 | |
| ….. | 24 |
Date Created: November 27, 2009
Last Revised: December 23, 2009
Public
Original Author: TO
All content © 1992-2009 Schneider Electric
Legacy KB System (APS) Data: RESL200782 V1.0, Originally authored by MiNe on 12/23/2009, Last Edited by MiNe on 12/23/2009
Related ranges: ION75X0 RTU, ION7550/ION7650, ION8800, ION8600
Publié pour: Schneider Electric Belgium