Issue:
The acceleration ramp is not smooth on the ATS48 soft start
Product Line:
Altistart 48
Environment:
All models and serial numbers
Cause:
The soft start is in torque control
Resolution:
Suggest to turn the torque control parameter to off. Go to the DrC menu, scroll down to the CLP parameter and set to off.
Publié pour: Schneider Electric Belgium