In SoMachine versions 4.1, 4.2 or 4.3 you can use the command located under the Logic Builder / Project / Compare to compare the actual project with another one (reference project). The reference project and the compare options are specified in the Project Compare dialog box, which opens, when the command is executed.
Publié pour: Schneider Electric Belgium