The VW3A31101 comes with the remote display, mounting screws, seal/cover for IP65 rating and a 3 meter cable. The cable is unique to this kit and not available separately. It has RJ45 and DB9 connectors.
Manual is attached.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Publié pour:Schneider Electric Belgium