Trip Circuit Supervision require a logic function to be created. In this example covering TCS with 2 inputs DI1 and DI2 is used for breaker open and close status. The inputs must be inverted (below NC selection). Please refer to manual for connections. For e.g. Easergy P3 standard, refer to chapter 6.16
Publié pour: Schneider Electric Belgium