Issue
Comparing Basic Configuration of M340 BMXNOC0401 & M580 BMENOC0301
Product Line
Modicon M580 BMENOC0301 M340 BMXNOC0401
Environment
Unity Pro DTM Browser
Resolution
Below is a video that compares the basic setup of a M340 BMXNOC0401 module with the basic setup of a M580 BMENOC0301 module.
Comparing Basic Configuration of M340 BMXNOC0401 & M580 BMENOC0301
Product Line
Modicon M580 BMENOC0301 M340 BMXNOC0401
Environment
Unity Pro DTM Browser
Resolution
Below is a video that compares the basic setup of a M340 BMXNOC0401 module with the basic setup of a M580 BMENOC0301 module.
Publié pour: Schneider Electric Belgium