Issue:
What is the part number for the substitution kit for ATV61/71 to ATV630/930?
Product Line:
ATV630 ATV930
Environment:
ATV630 ATV930
Cause:
Replacing ATV61/71 with new ATV630/930.
Resolution:
The part numbers for the mounting adapters are selected based on VFD frame sizes. These kits are used to install an Altivar Process Drive in the place of an Altivar 61 or Altivar 71 drive, using the same mounting holes. It includes the mechanical adaptors required for mounting.
See attachment.
Publié pour: Schneider Electric Belgium