Is it possible to connect non-referenced pulse energy meter in Smartlink ELEC ? How to configure the demand power?
It is highly recommended to use referred references in Schneider Electric catalogue.
If use non-referenced pulse energy meter, you need to make herebelow configuration.
Power = Energy/Time = (3600 x Weight of each pulse)/time is seconds between the 2 last pulses
This gives an average power calculated in the recent past, as it is calculated between the 2 last pulses received by the Smartlink EL B from the connected meter. The minimum width of pulse must be 50ms.
i.e., if 4 seconds between 2 last pulses, and weight is 10 Wh per pulse (in that example the unit is Wh), calculation will give 3600*10/4 = 9000 W
It is set to zero if no new pulse has been received after 3 times the time between the 2 last pulses.
Precision is 5% when frequency of pulses is less or equal to 5 Hz (5 pulses per second)
Publié pour: Schneider Electric Belgium
Besoin d'aide ?
Sélectionnez le bon produit
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.