Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Altistart 48 require separate control power?
Issue:
Does the ATS48 require separate control power?

Product Line:
ATS48

Environment:
All

Resolution:
Yes, terminals CL1 and CL2 require 90 to 270 Vac, 50/60 Hz to supply control power.
It is common to use 120 VAC to supply power for the ATS48 control power.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center