Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do the drawings in the ATS48 Installation Guide show 2 fuses on CL1,CL2 terminals?
Issue:
Drawings in the ATS48 Installation Guide show 2 fuses on CL1,CL2

Product Line:
ATS48

Environment:
All

Cause:
ATS48 fuse on the CL1 and CL2 terminals

Resolution:
It is not necessary to have two fuses. Only one fuse is needed. Please refer to attached Catalog for updated drawings.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATS48 Catalog October 2014.pdf [3.79 MB]