Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the ATS48 soft starters dissipated watts loss for calculating heat loss for enclosure sizing?
Issue:
Looking for the watts loss on a  ATS48 soft start

Product Line:
Altistart ATS48 soft starters

Environment:
All

Cause:
Needs to know the dissipated heat loss in watts the ATS48 soft starter will produce when running at full load.

Resolution:
See the table below and choose the ATS48's watt loss based on if a shorting contactor is being used or not.


ATS48 Watts Loss


Schneider Electric Egypt and North East Africa