Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the LED pilot light bulbs used in a Model 6 Drives MCC?
Issue:
Replacement LED pilot light bulbs for Model 6 MCC drives

Product Line:
Model 6 LVMCC

Environment:
All

Cause:
LED replacement

Resolution:
LED Bulb for 22mm type XB5 (plastic) or XB4 (metal), used for 110/120Vac
25501-00003 - Red LED
25501-00005 - Green LED
25501-00004 - Yellow/Amber LED
25501-00006 - Blue LED
25501-00007 - White LED

LED bulb for 30mm 9001 type K, used for 120Vac/dc
6508805210 - Red LED
6508805212 - Green LED
6508805211 - Yellow/Amber LED
6508805213 - Blue LED
6508805214 - White LED