Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the bulletin number for the startup and receiving manual for the Altivar ATV66 drive?
Issue:
Looking for the bulletin number for the startup and receiving manual for the Altivar ATV66 drive?

Product Line:
Altivar Machines, Altivar 66

Environment:
All models

Cause:
N/A

Resolution:
The bulletin number is VD0C06S304 "Constant and Variable Torque: 1 to 400 hp, 460 V and 1 to 50 hp, 230 V Receiving, Installation and Start-Up".Start-Up Bulletin: https://www.se.com/us/en/download/document/VD0C06S304/Repair Parts Addendum: https://www.se.com/us/en/download/document/30072-450-73/

Schneider Electric Egypt and North East Africa

Attachment(s)
Altivar-66-ATV66-User-Installation-Manual.pdf [1.34 MB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category: